Part Number: SN65DSI84-Q1
Other Parts Discussed in Thread: SN65DSI85-Q1
Hi, Team,
Customer is considering to use SN65DSI84-Q1 series to convert MIPI to oLDI because one of the output of Sitara is MIPI.
1. Is SN65DSI84-Q1 will be enough to output oLDI Dual 1920x1440 (110MHz x Dual) from MIPI 4 lane input?
2. Is SN65DSI85-Q1 a selector (which outputs either input DA/DB to dual output), a merger (merges 2 input into 1 and outputs via dual output channel)?
Thanks,
Masaru Oinaga