Part Number: DS90UB954-Q1
Hello Guys,
Good day.
Our customer is planning to use two camera inputs to DS90UB954 with different resolution and fps.In this case Two 953's are interfacing with different resolutions and frame rate., For example one input with 1080P @ 30FPS and other input with 480P @ 60fps.
Found from other forum thread that the DS90UB954-Q1 can be paired with different cameras having different resolution and FPS. However could you help with the inquiries below?
1) In this case, planning to use two different sensors , i believe no impact on the use case
2) What is a best topology ( 4 lane or 2+2 lane) for this use case, please suggest
Thanks and regards,
Art