Part Number: DS90UB954-Q1
We have been doing testing over temperature and from our observations we think it is possible our MIPI link between the 954 and our ISP processor may be the problem. As I lower the temperature, we appear to loose MIPI packets at the ISP input. We have extensively looked at the soldering of the devices and we feel confident that the assembly is now not the issue.
Two questions:
- What are the recommended settings for four lane, 1.6 Gbps link speed interface? Is periodic calibration recommended?
- Are registers 0x3B to 0x41 associated with the CSI interface? Are there any undocumented adjustments we can do with any of these registers?