This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Since an 8 megapixel Sensor is used in our subsequent scheme, can 953 be matched with 2 million ~8 million Sensor? Thank you!

Part Number: DS90UB953-Q1


1、Now we have received the development demand of 200W and 800W LVDS cameras. The sensors are matched with Sony's IMX415 and IMX462 sensors.

If you want to match the serial device with TI, please help to provide the camera scheme of FPD-Link III, thank you!

2、Since an 8 megapixel Sensor is used in our subsequent scheme, can 953 be matched with 2 million ~8 million Sensor? Thank you!

  • Hello Ken,

    Can you clarify what you mean about 200W and 800W? If you are looking for a serializer solution for CSI-2 cameras, can you please provide the CSI-2 lane speed required and the number of CSI-2 lanes for the specific sensor configuration you are looking at?

    Best Regards,

    Casey