Part Number: TUSB4041I
Other Parts Discussed in Thread: TUSB2046B
Are 27ohm termination resistors required for the TUSB4041I? The datasheet for the TUSB4041I doesn't mention that it has internal termination resistors. However, in the implementation schematics for the downstream connections, it shows direct connections to the USB type A ports. I noticed in the datasheet for the TUSB2046 that it requires 27ohm resistors on the P and N signals plus 15K to ground for each. I'm unsure if I need external termination resistors for the TUSB4041I.
Thanks
Chad