Part Number: DS90UB960-Q1
Hi Team.
My customer now use 953+960 together. The lock is unstable, sometimes high sometimes low.
I will ask customer to check the CLK whether it is ok.
At the same time, could you kindly help to check whether their configuration is ok? whether have problem based on this configuration?
UB960_ID,0x01, 0x01},//Reset
{UB960_ID,0x02, 0x3E},//GENERAL_CFG
//{UB960_ID,0x0C, 0xAB},//RX_PORT_CTL
{UB960_ID, 0x14,0x81}, // To configure GPIO0 to bring out Lock for Port0,
//{UB960_ID, 0x15,0xA1}, // To configure GPIO0 to bring out pass for Port0,
{UB960_ID,0x4C, 0x01},//FPD3_PORT_SEL PORT0
//{UB960_ID,0x4C,0x12}, //PORT1
{UB960_ID,0x58, 0xDE},//BCC_CONFIG
//{UB960_ID,0x58, 0xD8},//BCC_CONFIG
{UB960_ID,0x5C, 0x80},//SER_ALIAS_ID
{UB960_ID,0x5D, 0x32},//SlaveID[0]
{UB960_ID,0x65, 0x90},//SlaveAlias[0]
{UB960_ID,0x6D, 0x7C},//PORT_CONFIG
{UB960_ID,0x70, 0x1E},
{UB960_ID,0x6D, 0x7C},//PORT_CONFIG
//{UB960_ID,0x33, 0x21},//CSI_CTL
{UB960_ID,0x33, 0x01},//CSI_CTL
//{UB960_ID,0x20, 0x00},//FWD_CTL1
{UB960_ID,0x20, 0xE0},//FWD_CTL1
{UB960_ID,0x21, 0x00},//FWD_CTL2
//{UB960_ID,0x1F, 0x02},//CSI_PLL_CTL 修改
{UB960_ID,0x1F, 0x00},//CSI_PLL_CTL
{UB960_ID,0xB9, 0x1F},//LINK_ERROR_COUNT Len 15
{UB960_ID,0x6E,0xAA}, // BC_GPIO_CTL0: FrameSync signal to GPIO0/1
{UB960_ID,0x15,0x91}, // FrameSync signal; Device Status; Enabled
{UB960_ID,0x19,0x15}, // FS_HIGH_TIME_1
{UB960_ID,0x1A,0xB0}, // FS_HIGH_TIME_0
{UB960_ID,0x1B,0xC3}, // FS_LOW_TIME_1
{UB960_ID,0x1C,0x40}, // FS_LOW_TIME_0
{UB960_ID,0x18,0x01}, // Enable FrameSync
{UB953_ALIAS_ID,0x02, 0x13},//General_CFG
{UB953_ALIAS_ID,0x0E, 0x1E},//GPIO_INPUT_CTRL
{UB953_ALIAS_ID,0x0D, 0x01},//LOCAL_GPIO_DATA