Part Number: TCA9517
Other Parts Discussed in Thread: TCA9800
Hi,
I am using the TCA9517 on a 3.3V SM Bus (both sides). The Master is currently Connected on Side B, ans other Slaves are on Side A (all 3.3V).
The Datasheet example has the Master placed on Port A. But there is a text in the datasheet that the master can be connected on either sides. Is there a problem with the master on side B ?
Also I am seeing a offset on low levels for signal and clock on B Side of about ~600mV. This is not recongnized as low for the SMBUS device on side A. I am tried to increase the pullups but I can not get this low level down to ~0V. What causes this issue?
EDIT:
One more thing I need to say is that the A Side (that goes "outside") is connected with a pullup to the VCCB Side (internal) because both voltages should be identical. The Datasheet wants this to be connected to the VCCA side, but I do not have this exact voltage. Any problems here ?
Thanks