This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4E001: Differential signal connectivity

Part Number: TPD4E001

Hi,

I am using TPD4E001DCKR in my project. Is there any guidelines how the differential signals should be connected. Whether they can be connected to any pin.

I have connected signals as below.

Pair1_P to Pin.1

Pair1_N to Pin.3

Pair2_P to Pin.4

Pair2_N to Pin.6

For routing feasibility I have to change signal connection as below.

Pair1_P to Pin.3

Pair1_N to Pin.4

Pair2_P to Pin.6

Pair2_N to Pin.1

Is this correct.