Dear Expert
I have a question about the data rate of DS110DF410, I would like to consult the original factory, thank you!The details are as follows:
1. If the data output mode is set to RAW Data, the CDR circuit is not used.Whether the input and output rates are still limited to 8.5Gbps to 11.3Gbps and their sub-rates of 1/2, 1/4 and 1/8.If there is no limit, then what is the input-output rate range at this point?