This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Setting power sourcing to different value than is advertised

Part Number: TPS25750
Other Parts Discussed in Thread: BQ25731

When using with a BQ25731 as a battery pack sourcing power we'd like to set the circuit to provide 100W but only advertise up to 60W.

If in the GUI under 'Questionaire' we set '2.What is the maximum power that can be sourced?' to 100W and then under 'Configuration' set the PDO for 20V to 3A, will this accomplish this?

Thanks!