Part Number: TUSB2077A
Hello,
1) I was wondering about an APLL.
On page5 "datasheet", PIN Functions: MODE -> Mode select. When MODE is low, the APPL output clock is selected as the clock source ~~~
what is the full name of APLL?
2) Question number 11 on the "TI USB 1.1/USB 2.0 Hub Frequently Asked Questions", we have to pull down to the ground if unused downstream ports exist.
Then, 15KOhm is enough for a pull-down resistor value?
Thanks for reading.
And I'm looking forward to your reply.