Part Number: TPD4E110
Hi,
From pg. 10 of the datasheet, what is the in-pad GND vias hole size and diameter?
Do you mind sharing the Altium PCB file for the EVM?
-kelvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD4E110
Hi,
From pg. 10 of the datasheet, what is the in-pad GND vias hole size and diameter?
Do you mind sharing the Altium PCB file for the EVM?
-kelvin
Hi Kelvin,
I don't have an exact measurement for the GND via on page 10. However, I would say that the via should be no larger than 0.25 mm in diameter since that is the length of the GND pad on the device.
The Altium file can be downloaded here: https://vendor.ultralibrarian.com/TI/embedded/?gpn=TPD4E110&package=DPW&pin=4&sid=017a1a937e5700115cb064e0b05403073001b06b00bd0&c=1
Regards,
Matt Smith