This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[SERDES] Part recommendation request

Hi, TI Support Team

The customer company is reviewing development as shown in the block below.

- MIPI to GMSL2 Dual type (Serializer) , I2S Input/Output support

- GMSL2 to MIPI dual type (Deserializer) , I2S Input/Output support

- HDMI to GMSL2 Switch (1:2) , I2S Input/Output support

- GMSL2 to HDMI Switch (2:1) , I2S Input/Output support

- GMSL2 to HDMI Converter , I2S Input/Output support

Please recommend applicable products.

GMSL2 is considered the same as FPD-Link3, and please recommend a product that supports Full HD.

In addition, if there are parts applicable to the structure below, please recommend.

MIPI to GMSL2  --> GMSL2 to LVDS --> LVDS to HDMI Converter --> HDMI Mux Switch (2:1)

Thanks.

Regards,

MJ

  • Hi MJ,

    MIPI to FPD-Link III , I2S Input/Output support: DS90UB941AS

    FPD-Link to CSI , I2S Input/Output support: DS90UB940N

    HDMI to FPD-Link III , I2S Input/Output support: DS90UB949

    FPD-Link III to LVDS, I2S Input/Output support: DS90UB948

    There is no device for FPD-Link III to HDMI.

    TI does not have a device that will do LVDS to HDMI Converter. 

    Regards,

    Michael W.

  • Hi, Michael

    Thank you for reply.

    I have recommended products to customers with the following blocks.

    Please check whether the parts applied to each sector are appropriate.

    Thanks.

    Regards,

    MJ