Part Number: TDP158
Other Parts Discussed in Thread: TMDS181
Hi sir,
My customer use TDP158 as HDMI redriver on intel Elkhart lake platform and they have question about HDMI level shifter configuration on bios setting: If they set the level is 450mV (as default), the max output resolution is 1080p. But if they adjust it to 850mV, they can get 4K video signal. We see they have ac couple capacitor on board. Do they still need external termination to 3.3V between the HDMI source and AC cap as the previous post suggestion? And any suggestion for the pull up resistor? Thanks for your kindly help.
Best regards,
Gary Teng