Part Number: TUSB321
Hi,
Customer need a ref circuit of TUSB321 working as a UFP. could you please support this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yue,
TUSB321AI UFP schematic is very similar to DFP example in datasheet. In this case PORT is tied to GND with 4.7k. Current_Mode, VCONN_FAUL and ID are not used. All other pins can be used as directed (OUT1 and OUT2 are optional open drain outputs).
Malik,
without power supply on VDD pin, as a UFP, is the Rd inside TUSB31 still avaiable? based on my undestanding, VBUS has no voltage at first, then after CC , VBUS will have voltage, then TUSB321 can be powered by VBUS. right? I mean TUSB321 doesn't have to be power at first if internal Rd is avaiable, once CC process done, them VBUS will be able to power TUSB321.