Part Number: TUSB7320
Please let me know if there is a register that can adjust the drive capacity of D + (USB_DP_DN2) and D- (USB_DM_DN2) of TUSB7320.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB7320
Please let me know if there is a register that can adjust the drive capacity of D + (USB_DP_DN2) and D- (USB_DM_DN2) of TUSB7320.
Please tell me the drive capacity (XX [mA] as an example) for D + (USB_DP_DN2) and D- (USB_DM_DN2) of TUSB7320.
Also, with this terminal, does the drive capacity change between startup and steady operation?
In addition, please tell me about the drive capacity.
Is it possible to change the drive capacity of D + (USB_DP_DN2) and D- (USB_DM_DN2) at startup and during USB communication (previous answer)?
The intent of the question is that when determining the USB communication mode (high speed as an example), D + and D- operate on a single end rather than a differential signal.
At that time, an undershoot occurs in the signal on the device side.
We are investigating whether there is a countermeasure to suppress undershoot.
HI,
Unfortunately there is no ability to change drive capacity at startup. Could you share waveform here for review?