Other Parts Discussed in Thread: TB5D2H
The SN65LBC173A has internal pullup/pulldown resistors on both inputs.
From the functional block diagram, it looks like 100kΩ pullup, a series 18kΩ resistor, and then another few kΩ pullup and pulldown.
The other input has the resistors attached to the other rail (GND).
I need to know how a driver like TB5D2H would perform...it only has "high-side transistors" and supports 150Mbps, but my customer only needs to achieve ~ 22Mbps.
With just high-side transistors, pulldown resistors are needed for device to have a proper output when one or the other transistors is OFF.
Is there a SPICE model available for SN65LBC173A?
Is there an equivalent pullup/pulldown resistance value you can help me calculate for each of the two input lines for a Channel?
Please understand I need a reply to this question - sometimes I get pointers to other devices, etc, but for this time in particular I really need an answer to the above
Regards,
Darren