Part Number: TFP410
Let me ask you two questions below.
①
If I input an irregular resolution and frame rate to the TFP410, will the TMDS encoding be an error and will not be output?
For example, in the case of 480x 272, the pixel clock is 25MHz or less, so take a lot of blank period.
If a signal such as adjusting the pixel clock to 25Mhz or higher is input, no video will be output even if a DE signal is input with the hardware PIN setting.
However, it is output when I2C is set to generate DE.
From the CVT standard, the polarities of HSYNC and VSYNC change depending on the resolution and refresh rate.
Input signal analysis is included internally,
I think it is an error, but is it interpreted correctly?
②
Even with an irregular resolution refresh rate, if it is set to generate DE with I2C, it will be encoded according to the set register, so
I think that the image will be displayed if the Display side supports it.
Is this the correct way to use TFP410?