Part Number: DP83869EVM
Other Parts Discussed in Thread: DP83869HM, DP83869, TIDA-00306
Hello
we want to design DP83869evm to send data using the 100 Mbps Media Converter.
The setup is the following.
PC 1 ---------------------> Ethernet ---------------------> RJ45 connector DP83869EVM ----------> Media converter ---------------------> SFP cage + SFP connector Ethernet -----------------> PC2.
The speed of the ethernet link is set to be align with the 100 Mbps. The PC are windows computer.
The main objective is to use the DP83869HM as a media converter Copper Fiber and transmit directly information with only strap configuration.
However, based on the following configuration we are not able to transmist information, there is no answer when pinging both computer. we used the following configuration for the strap :
100 Mbps Media Converter
JTAG_TDO / GPIO_1 -> OPMODE_0 : Pull-up to VDDI
RX_D3 OPMODE_1 : OPEN
RX_D2 OPMODE_2 : Pull-up to VDDI
LED_1 : AUX_IOVDD
LED_ 2 : AUX_IOVDD
RX_CTRL / MIRROR_EN : Cooper Miror Enable
RX_CLK_LINK_LOSS : Link Loss pas thru Disabled
My question are the following.
- I saw on the forum that is was possible to use the media converter configuration with only the strap configuration. Can you please confirm that it is possible ?
- Do you see any falws in our configuration or any data that need to be configure ? Do you have any idea to fix the problem ?
- We use the USB software for debug purpose, is there any register we can check in order to confirm that the link is up or not ?
Any other help will be appreciated.
Best regards,
Ynouss DIALLO