Part Number: SN65HVD1781
Hi Sir/Madam,
We are currently using SN65HVD1781 in our design. We would like to test the Bus Fault protection up to 60V of the part. What is the timing of the 60V voltage level we can provide to IC without damaging the component. Is there any other protection we need to follow to avoid damage to the board? What is the current limit we need to set for 60V power supply?
If any test setup is available please share it so the same can be followed to protect the IC or board from damage.
Regards,
M Amarnath