Part Number: DS125BR401A
Dear team,
Could you help answer below questions?
1. Will you suggest the PCIE Redriver is close to CPU or TBT?

2. Whether the 2.5GHz is corresponding to 5GT/s speed?

Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125BR401A
Dear team,
Could you help answer below questions?
1. Will you suggest the PCIE Redriver is close to CPU or TBT?

2. Whether the 2.5GHz is corresponding to 5GT/s speed?

Thank you.
Hi Rachel,
1). Let's put DS125BR401A close to the CPU. Note:
CPU TX should go to the A side input of the DS125BR401A. We should have 3-4dB loss - at minimum between CPU and the A-side input of the BR401A.
CPU RX would get connected to the BR401A B-side TX. We need to make sure insertion loss is within the limit of the BR401A as noted in the data sheet.
2). Yes your understanding is correct. 2.5GHz corresponds to the 5Gbps or PCIe Gen2 data rate.
Regards ,,Nasser
Hi Nasser Mohammadi,
Thank you for the quick reply. I will confirm them with customer.
Thank you.