Part Number: TUSB4020BI
I'm planning to use TUSB4020BI in my design. And I have several questions:
- The GRST require a minimum low duration of 3 ms. In the reference design tidrlt6, it simply place a 1uF capacitor on this pin, as there are already a pull-up in the chip, so I guess it combine with the pull-up in the chip to generate the delay. If so, is it safe to use 1uF capacitor in my design? And what's the value of the pull-up in the chip?
- I'm planning to use the chip without external configuration interfaces (no EEPROM and no SMBus) but with power switching function, such as overcurrent protection, is it possible?
Thanks.