Part Number: PCA9306
Other Parts Discussed in Thread: ISO1640,
Greetings!
In my customers application two 3.3V power domains are used. I2C signals need to be passed through these domains.
Will this part still prevent back feed current in an application where V1 and V2 have the same source but come up at 100ms difference, i.e. V2 comes 100ms after V1 but both have same GND?
I received feedback that the ISO1640 device can do this, however I wanted to verify that the PCA9306 can as well.
Thanks so much,
-Christian Greeff