Part Number: TCA9517A
Hi Expert,
Customer have a question about I2C signal undershoot.
They found the undershoot on I2C SDA line at ACK timing, like as below,
It was over than -0.5 (abs max).

They check several board and several times.
It seems to be from -600mV to -750mV / 25ns to 35ns.
Customer tried to add dumping resistor, however it was not improve well.
Question1, Does the waveform undershoot have any issue on the TCA9517A?
Question2, The worst undershoot is -750mV/ 35ns on their system. is it any problem?
Question3, Do you have any idea for the acceptable range for this undershoot?
Thanks
Muk