Part Number: TCAN1145-Q1
Hi Team,
For the TCAN1145-Q1, I have a couple of questions.
1. Can the wake pin for the TCAN1145-Q1 be connected to ground?
2. Under voltage :
- For the device, there are three power sources, 12V Battery, 5V and 3.3V
- The requirement is that the CAN communication should work at battery voltage 6V. Considering various tolerances and drops, the voltage at the VBAT pin would be 5.4V
- The CAN VCC is supplied from the 5V DCDC converter, which has its own tolerances and can drop down to 4.7V. In this case, the CAN device will be in under voltage condition, which will set a UV flag.
- When the UV is detected, can all the CAN information be read via SPI? This information is needed to know the state of the device (UV or not UV) and when exactly the device comes out of the UV condition and CAN messages can be sent again. Can you kindly advice on this state of the device.