This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Cannot detect plug state

Part Number: TPS25750

Hi team,

 

Our customer is facing the problem that the device cannot detect plug state appropriately after the clear Dead Battery Mode.

Could you kindly advise how to do it ?

 

They see the issue in the below condition.

  • TPS25750 is connected to USB device (USB2.0) and Tablet (USB PD, USB2.0)
  • The tablet is sink of USB PD / DFP, EVM board is source of USB PD and USB device is UFP

 

Procedure

  1. Those are connected as below in the situation that is not turned ON power supply.
    USB – EVM – tablet
  2. Turn on only USB device and tablet.
  3. After that, turn on EVM.

 

At 2. Situation, USB device and tablet can communicate with USB2.0

At 3. Situation, customer expectation is that the EVM is getting as source and table is getting as sink and then the EVM charge the tablet but the EVM isn’t able to charge the table.

 

Customer confirm that after power supply, the EVM is getting dead battery board and then enter DBfg command to TPS25750 and Dead Battery Mode is able to be cleared.

 

When Dead Battery Mode is cleared, STATUS Resister bit 0 shows No plug is connected, and it isn’t able to detect connecting the tablet.

Therefore, it isn’t able to be source by Role Swap.

 

We would much appreciate it if you are willing to give us any advice.

Thank you and best regards,

Michiaki