This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA39306-Q1: Eco Plan + Lead Finish / Ball material + Automotive Grade

Part Number: TCA39306-Q1

Hello, 

Is the TCA39306-Q1 ROHS, halogen and Lead Fee ? 

Is the component complient with Automotive standard AEC-Q100 ?

Regards, 

  • User,

    Please see TI's environmental page here for statements on RoHS (which includes lead) and halogen for TI parts. Our newest I2C devices are RoHS and REACH compliant.

    The Q1 at the end of the part number implies that the device went through the AEC-Q100 qualification process, so this device is indeed compliant with AEC-Q100.

    Regards,

    Eric Hackett