Part Number: DS90UH941AS-Q1
What is the data rate (rate) for single link and dual link of FPD-Link III? (for forward link and reverse link)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH941AS-Q1
What is the data rate (rate) for single link and dual link of FPD-Link III? (for forward link and reverse link)
Hello Kijung,
This is listed in the front page of the 941AS datasheet. The single link max PCLK is 105MHz (3.675Gbps), dual link max PCLK is 210MHz (3.675Gbps/lane).
You must also consider the max PCLK capability of the specific deserializer that you plan to pair with as well. This can be found in the respective datasheet for the deserializer
Best Regards,
Casey