Other Parts Discussed in Thread: TPS25981, , BQ24172, TPS65987D, TPS65981
Hi Team,
Right now i am working on the register configure on 0x33 TX_SINK_CAPS Register.
But it's seems not son clear acording to the TRM.
- Does the 7 PDOxS have a fixed order and cooreasponding to the source side?
- If I only wang a SINK with 45W/3A, shall I only congifgure the 15V/3A PDO and the forst PDO? The other bits only need to set to "0" will be ok? Or "1"?
-There are 7 PDOs listed in TRM, Which PDO is cooreasponding to 15V/3A?



Thanks,
Best Regards,
Matt