This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: DP83867IRRGZR VIL levels at 1V8 IO

Part Number: DP83867IR


Dear sir/madam,

Datasheet of DP83867IRRGZR states that when IO voltage of 1V8 is used the VIL max threshold -> 0.2 * Vcc = 0.36V. Is this correct? This seems really low and makes it virtually impossible to correctly interface with other devices (for example Xilinx 7 series FPGAs have VOL max of 0.45V at 1V8 IO levels).

Kind regards