Other Parts Discussed in Thread: SN75DP159, TDP158
for our Network Video recorder project we want to convert Dual mode DP++ port of Elkhart x6413E processor to HDMI connector output.
Please suggest IC for Display Port Dual mode receiver to HDMI 2.0 transmitter
Specifications:
Accepts Dual mode DisplayPort 1.4 output from Elkhart x6413E processor having. Support for 1/2/4 lanes at 1.62(RBR)/2.7(HBR)/5.4(HBR2) Gbit/sec per lane To
HDMI 2.0 (4K@60Hz) transmitter, up to 6.0Gbit/sec per TMDS data channel.
Not able to decide which type of IC should be used, Retimer or Redriver?
KIRAN SURVE