This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100MB203: LVCMOS I/O questions

Part Number: DS100MB203


Hello,

Q1:
When 3.3-V mode, is VDD pin voltage 3.3V?

Q2:
LVCOMS Voh and Vol spec is the same regardless of whether 2.5-V mode or 3.3-V mode?

Best regards,

K.Hirano