Other Parts Discussed in Thread: TCAN1044V
hello, sir,
this is eric.li, an EE engineer from Advantech Co. Ltd.
we choose STM32F405 as CAN-MCU and SN65HVD251 as CAN transceiver.
the Voh of MCU's TX is 2.9~3.3V but the Vih of D input of CAN transceiver is 3.5V (0.7*VCC).
although the Voh of STM32F405 violates the min. Vih 3.5V of SN65HVD251, in our internal function and throughput test, it works fine as expected. see table.1
we wondered if SN65HVD251 can accept D input lower than 3.3V, even to 2V?
thanks a lot !
Regards,
Eric Li
Table.1 CAN bus throughput test result, for STM32F405 as CAN-MCU and SN65HVD251 as CAN transceiver