This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0074: Carrier Detect with HD-SDI input

Part Number: LMH0074

I am looking for some clarification regarding the Carrier Detect output of the LMH0074. What would the state of CD be if a 1.485 Gbps HD-SDI signal is present at the equaliser input?

Since the LMH0074 is a 270 Mbps SD-SDI equaliser, I would expect CD to remain high (no signal).

Is the state of CD based purely on input signal amplitude or does it also take into account the input signal bit-rate?

Thanks.