This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: More information on Built In Self Test (BIST)

Part Number: DP83869HM

I am looking for more information on how to use Built In Self Test (BIST) on the DP83869HM.

  • What is the sequence of register writes to enable MII Loopback, use the PRBS generator, and the TX checker?
  • When using the PRBS generator, what is the packet size?
  • With reference to page 79 of dp83869hm.pdf, bits 7 and 8 of PRBS_TX_CHK_CTRL Register. There is a note saying “Writing bit 7 generates a lock signal for the PRBS TX counters. Writing bit 8 generates a lock and clear signal for the PRBS TX counters.” I am not sure exactly what it means by “lock and clear”. Does it mean to lock it at 0?
  • How do you disable the lock on the PRBS_TX_CHK_BYTE_CNT register after it has been locked by setting either bit 7 or 8 of the PRBS_TX_CHK_CTRL Register?

If there are any application notes or better documentation of how to use BIST, I would greatly appreciate it if you could send a link to me.