This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3243: lowest supply voltage

Part Number: MAX3243

Hi Team,

Customer would like to double check what is lowest legal supply voltage for this device?

The lowest voltage customer observed on their system during power rail swap is about 3.9V.

They found at this voltage, communication seems still fine, thanks for checking.

The spec said Vcc = 3.3V, MIN is 3V, Vcc = 5V, MIN is 4.5V. So if lowest voltage is 3V or 4.5V? 

Thanks.

Andrew