This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: What will be Propagation delay at 12Gbps data rate of TMUXHS4212 internal switch/body ?

Part Number: TMUXHS4212

Hi Sir,

We are using TMUXHS4212 in our HDMI 2.1 interface and as per HDMI 2.1 standard, it will work up to 12Gbps datarate. 

During net length matching and max track length calculation, we required propagation delay value at 12Gbps. In datasheet, it is mention at 1Gbps only.

Can you please let me know propagation delay value at 12Gbps? as well as can we swap P&N polarity in mux?