Part Number: TPS65988
Hello TI Team,
we recently fixed a hardware bug in our system where our TPS65988 as a PD source only on both ports was being back-powered due to some leakage (powered by the sink).
But now, with the correct power sequencing (user powers on system, 5V and 3.3V rails are generated, 3.3V supplies the 3.3V_LDO rail), the SPI flash is not correctly read, even though it was previously.
Our suspicions are on the flash data out signal pull-down R12 (SPI_POCI in the datasheet). With it removed (no pulldown or pulldown), the flash was able to be read in the abnormal power conditions. Now, it can't be read when R12 is open, 1k, 3k or 10k.
The desired Boot config is BP_NoResponse Config1 (SPI_POCI =0, DIV=0.14)
Do you maybe have any ideas on the expected R12 value or see any other problems?
Thanks,
Daniels