Part Number: TCAN1145-Q1
Hi Team,
From the following link, it is confirmed that WUF of TCAN1145 must be a standard CAN frame.
my question is do we have any devices to support CAN-FD Frame remote wake up?
B&R
Lijia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1145-Q1
Hi Team,
From the following link, it is confirmed that WUF of TCAN1145 must be a standard CAN frame.
my question is do we have any devices to support CAN-FD Frame remote wake up?
B&R
Lijia
Hi Lijia,
No, there are no TI devices that support remote wake on CAN-FD frames. It is my understanding that this feature is not available in any device currently on the market as this behavior is not defined in the selective wake definition of the CAN standard. I don't expect that this behavior will be developed as it adds significant complexity to the transceiver without a direct benefit to the selective wake feature.
If this request is coming from a customer based on an end-requirement, I would encourage the customer to push-back on this requirement as the behavior is not defined and would not provide direct benefit to the selective wake feature.
Regards,
Eric Schott