Hi.
I have a question the behavior of Linkup Status on Basic Mode Status Register (BMSR).
[Schematics]
FPGA <-> DP83822HF <-> SFP module for 100BASE-FX (*) <-> fiber cable ...
*) Finisar FTLF1217P2BTL
[Procedure & the behavior of Linkup Status]
1. Power-On without the fiber cable
=> BMSR : 0x7849 => bit2 is 0 = Link not established
2. Inserted the fiber cable & connect to other device
=> BMSR : 0x784D => bit2 is 1 = Valid link established
3. Removed the fiber cable
=> BMSR : 0x784D => bit2 is 1 = Valid link established
* I expected bit2 is 0.
[Question]
The behavior of Linkup Status is the DP83822HF's specification? (normal? or abnormal?)
Because, re-inserted the fiber cable after above procedure3, the packet data's lost is incresed on 100BASE-FX.
Is it available to re-insert the fiber cable?
Or, is it neccesary to reset DP83822HF or set the specific register?