Part Number: DP83TD510E
Hi Team,
I have two questions from customers.
Question 1) What is the required specification of the cable to be used?
I understand that there is more flexibility in cable selection than standard Ethernet.
I would like to know if the vinyl cabtyre round cord (VCTF2C-0.5SQ) used in the transmission cable of the existing system can be used.
*The communication distance is about 25m.
Question 2) If set the Input Clock to 12.5MHz, will it work? (The opposite PHY is assumed to be set at 12.5MHz.)
The customer doesn’t need a transmission speed of up to 10Mbps.
Regards,
Kenji