Part Number: SN65HVD3082E
Dear Specialists,
My customer'd like to obtain a graph of the differential output current value when Vcc changes.
Data sheet P.8 Figure 6-5. Driver Differential Output Voltage versus Driver Output Current only describes Vcc = 5V.

They want a graph with the characteristics when Vcc = 5.5V and 4.5V.
The graphs of other company is shown for reference.( The other maker's product)

If possible, it would be nice if there was data when Vcc = 4V in addition.
They are investigating differential output current change and Vcc.
I appreciate your great help in advance.
Best regards,
Shinichi