This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does TI have a P2P or similar solution to V5.5MLA0603N and SMF4L6.5A?



Hi team,

Does TI have a P2P or similar solution to V5.5MLA0603N and SMF4L6.5A? 

V5.5MLA0603N use in USB 5V.

SMF4L6.5A use in battery input.

  • For the USB 5V VBUS you could use the TPD1E10B06 which is comes in two packages - and I would particularly recommend the  0.6mm2 0402 (TI - DPY package) and has a 6A Surge rating

    SMF4L6.5A  - I would also recommend theTPD1E10B06 especially in the leaded SOD-523 which is much smaller than the SOD-123 package.

    If you require a higher surge rating for both devices I would recommend the TVS0500