Part Number: TCAN4550
Hi,
How to validate the Internal Loop Back Test Mode ?
Is there any procedure to validate this ? if there please suggest the same.
Best Ragards,
Manu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Manu,
The internal loopback test mode can be used to test the CAN controller settings for the device without the use of external electrical connections to a CAN bus. This simplified setup allows for validation of configuration settings without the added complexities of an external physical system. There is no specified test procedure to validate this test mode as it is meant to be used to test desired controller configurations.
Let me know if this is clear and if you have any more questions.
Regards,
Eric Schott
Manu,
Yes, the intention of this mode is to test the controller configurations. So, you can test the SPI configuration and messaging capabilities by configuring the controller as you normally would, and then "transmitting" a CAN frame. If the CAN frame is "received" by the storage element you configured, and an interrupt gets asserted, then you'll know you configured it correctly.
Regards,
Eric Hackett