Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: DS90UB921-Q1, , DS90UB921-Q1EVM
Hello.
I have a DS90UB921-Q1 serializer and a DS90UB948-Q1 deserializer. They are connected by a coaxial cable. I am using fackra FA1-NZRP-PCB-8A connectors and RG-174 / U coaxial cable. The deserializer DS90UB948-Q1 is connected to a 1920 x 720 pixel display.
When the display is turned on, there is a rattling of the display image. At this moment, the "lock" signal becomes "0". When the image stabilizes, "lock" becomes "1". Also, the display may flicker and not turn on; after turning on the power again, the picture on the display will stabilize.
I only see this problem when the deserializer is connected with a coaxial cable. When I use the twisted pair, everything is fine.
Tell me what could be the problem.