This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044A-Q1: Could TCAN1043 & TCAN1044 layout replacement?

Part Number: TCAN1044A-Q1
Other Parts Discussed in Thread: TCAN1043

Hi Team,

There is a good new that we could DIN TCAN1044A!

Customers currently have a very urgent out of stock problem!
Originally recommended TCAN1043 to replace NXP products! But currently there is only TCAN1044 on hand! Is there any way to TCAN1044 layout replace TCAN1043 ?

  • Hi Kygo,

    TCAN1044 is an 8-pin transceiver and can't support the Sleep mode features of TCAN1043 which has 14-pins. However, the top 8 pins of these devices are functionally equivalent so a TCAN1044 would be able to fit the same footprint if the system can be adapted to only use Standby mode. 

    Regards,
    Eric Schott

  • Hi Eric,

    This is a good news!

     I will first confirm that customers need the Sleep mode features?
    If not , I will share this information with customers! And get the SCH after this! THX