Part Number: TUSB9260
Other Parts Discussed in Thread: TUSB9261
Hello, I have a problem with the chip TUSB9260. When I connect the device (SSD), PWM0 is on all the time on DEmoboard, PWM1 blinks, GPIO2 blinks, the device is seen in Windows Device Manager as a drive, in Disk Management flashes a drive with the correct memory size but in RAW format
DeviceInstanceId USBSTOR\Disk&Ven_&Prod_TS32GSSD370S&Rev_2B\1234123412341234&0
DriverName disk.inf
ClassGuid {4d36e967-e325-11ce-bfc1-08002be10318}
ServiceName disk
LowerFilters
UpperFilters
Problem 0x0
Status 0x0
DeviceInstanceId USBSTOR\Disk&Ven_&Prod_TS32GSSD370S&Rev_2B\1234123412341234&0
DriverName disk.inf
ClassGuid {4d36e967-e325-11ce-bfc1-08002be10318}
DriverDate 06/21/2006
DriverVersion 10.0.18362.1
DriverProvider Microsoft
DriverInbox true
DriverSection disk_install.NT
DriverRank 0xff0006
MatchingDeviceId GenDisk
OutrankedDrivers disk.inf:GenDisk:00FF2002
DeviceUpdated false
Status 0x0
ParentDeviceInstanceId USB\VID_0451&PID_9260\1234123412341234
I hope you can help.