Hi,
I want to test the IS2 function of 927/928. Can I use 927 and 928 to transport I2S signals without video input?
If I only provide I2S signals to 927, can I get the right signals from 928's I2S pins?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to test the IS2 function of 927/928. Can I use 927 and 928 to transport I2S signals without video input?
If I only provide I2S signals to 927, can I get the right signals from 928's I2S pins?
Thanks!
Hi Cathy,
You should be able to send I2S signals from 927 to 928 without video input.
You can find more information about I2S setup and config in this application note.
Regards,
Logan