Hello,
We are using the LVDS receiver DS90LV048A in a point to point application and need to have an output LOW when the input is unplugged (the differential input is terminated with a 100R resistor next to the receiver).
Under the "Fail-Safe Feature" tittle in the datasheet, says: "The internal fail-safe circuitry of the receiver is designed to source or sink a small amount of current".
Do you know the value of this current or, even better, the value of the internal pullup and pulldown resistors? I mean the R1 and R3 but inside the IC:

With that in mind I think it is possible to calculate the value of the external pullup and pulldown resistors to make the output low when the differential input is 0V.
Best regards,
Santiago