Part Number: DS90UB948-Q1
Hello TI,
We use DS90UB949 and DS90UB948 chips.
When the input signal of UB949 FPD-LINK is abnormal (for example, only FPD-LINK has a set of abnormal signals), can UB948 detect the abnormal signal?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Hello TI,
We use DS90UB949 and DS90UB948 chips.
When the input signal of UB949 FPD-LINK is abnormal (for example, only FPD-LINK has a set of abnormal signals), can UB948 detect the abnormal signal?
Hi Jinsheng,
The 949 to 948 link has a lock register/pin that verifies the deserializer's PLL is locking to the forward channel data/clock. Also, the Pass pin also identifies some faults or corrupt display timing/data on the link. Additionally there is also a link error counter (register 0x41) that monitors errors in some of the control/overhead bits.
Regards,
Logan